Use Pre-defined Libraries

The Libraries toolbox allows you to select the functions.

For an exhaustive list, refer to:

Drag-and-drop into the editors

  1. When the function is selected, move it with a drag-and-drop operation in the program editor
  2. In the editor, right-click on a function to set the number of input pins if the block allows an extension.
    Set the Pins Number of the Block
  3. Figure 5-35: Set the Pins Number of the Block

Drag-and-drop into the dictionary

If you have selected a function block, you can drag-and-drop it in the program declaration within the Dictionary toolbox, to create an instance of that object.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen